Options in the Single Import File dialog box
The following table shows options in this dialog box.
Options | Description |
---|---|
Select the single display import file to use | Click the browse button to open a search dialog where you can navigate to the graphic XML file you intend to import. |
Select the display to import to | From the list, select the name of the display you want to modify. All the displays in the application are listed. |
Create new objects on the display | Choose this option if the XML file you are importing creates new objects on the specified display. |
Update existing objects on the display | Choose this option if the XML file modifies the properties of objects already on the display. |
Provide Feedback