LinkConnections or (GroupLinkConnections)
The LinkConnections property specifies whether or not the reference object will use the connections assigned to the base object.
If the property is True, the object's connections will be read-only, and cannot be edited. This is the default.
If the property is False, the reference object can have other connections assigned. These connections will not affect the base object, and any changes to the base object's connections will not be picked up by the reference object.
Only reference objects that support a connection will have a LinkConnections property.
TIP:
In FactoryTalk View Site Edition, a reference object that is a tag label, trend, or Button with an action other than Command, always uses the connections assigned to its base object. You cannot set up connections for these reference objects separately.
Provide Feedback