Edit the Link properties for a reference object
The Link properties are given default values when the reference object is created. You can edit these properties for a given reference object in the
Property Panel
.To edit the Link properties:
- Right-click the reference object and selectProperty Panel.
- In theProperty Panel, click a property and edit the option.
Provide Feedback