Change default values for the Link properties

The Link properties are given default values when the reference object is created. You can change the default values that are assigned to a reference object when it is created.
To change default values for the Link properties:
  1. Right-click the reference object and select
    Global Object Defaults
    .
  2. In the
    Global Object Defaults
    dialog box, specify the new default values.
  3. When complete, click
    Apply
    or
    OK
    . The new default values will be applied to all new reference objects, as they are created.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal