Break links between a reference object and its base object

You can break the links between the reference object to its base object. When you do this, the reference object becomes a standard graphic object.
Do one of the following to break the links:
  • Right-click the reference object and select
    Break Link
    .
  • Delete, remove, or rename the global object display containing the base object.
  • Delete or rename the base object itself.
    TIP:
    If you delete an object that is part of a grouped based object, the corresponding object in the grouped reference object is also deleted, instead of being treated as a broken link.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal