Logging on to an SE application from an SE Client
To log on to a
FactoryTalk View SE
Client, the user logging on must be:- In theFactoryTalk ViewRuntime Security accounts list.
- Allowed to run applications in theFactoryTalk View SEClient.
When you install
FactoryTalk View SE
software, the All Users account is added
automatically to the FactoryTalk View SE
Runtime Security user accounts list. This
gives all users full access to FactoryTalk View SE
applications at runtime, without
needing to log on.If FactoryTalk Security has been used to apply additional security to an application at the
FactoryTalk Directory, the Login dialog box will be displayed when the
FactoryTalk View SE
Client is started, if any of the following is true:- Single sign-on is not turned on.
- Single sign-on is turned on, but there is no user logged on to the Factory Directory, and the current Windows user is not set up as a FactoryTalk Windows-linked user.
- Single sign-on is turned on, but the current FactoryTalk Windows-linked user does not have the necessary security permissions to run theFactoryTalk View SEClient.
If single sign-on has been turned on, and there is already a user logged on to FactoryTalk
Directory, the system checks that user's credentials first, when the client starts up.
If the current user is in the
FactoryTalk View
Runtime Security user accounts list
and has been granted the appropriate FactoryTalk Security permissions, no further log on is
necessary and the FactoryTalk View SE
client opens without the Login dialog box
being presented.Once logged in successfully, whatever
FactoryTalk View SE
security codes that have
been assigned and FactoryTalk Security permissions that have been set up, are in effect. All
commands issued from the client, including commands in macros, are checked against the codes
assigned to the user who is logged on.If the user attempting to log on is a Windows-linked user, they must provide the domain name with the user name, if the Windows-linked user is on a different domain than the Windows Desktop user, using this syntax
domainName\userName
.If single sign-on is turned on, changing the
FactoryTalk View SE
Client user does
not change the user currently logged on to the FactoryTalk Directory. To change the
FactoryTalk user during the current Windows session, use the Log On to FactoryTalk
utility. To start this utility, select Start
> Rockwell Software
>
Log On to FactoryTalk
.For more information about FactoryTalk Security,
FactoryTalk Services Platform Help
or FactoryTalk View
Site Edition User's Guide.Provide Feedback