Using single sign-on
Single sign-on is part of the security policy settings and is managed by FactoryTalk Security. The default setting is for it to be turned on. Single sign-on gives a user access to multiple products in a FactoryTalk-enabled system, without having to log in separately to each product.
For example, after a user logs into FactoryTalk Directory, either by starting and logging into FactoryTalk View Studio, or by using the Log On to FactoryTalk utility, when they start another FactoryTalk-enabled product, the login dialog will not be displayed.
The reason for this is that after the initial login, when another FactoryTalk-enabled product is started, FactoryTalk Security checks the credentials of the logged-in user at the FactoryTalk Directory, and authorizes access to the next product without requiring another log in.
Single sign-on authorization will be in effect for the logged-in FactoryTalk Directory user for the duration of the current Windows session, or until the user logs off the FactoryTalk Directory.
To confirm the setting of single sign-on:
- InFactoryTalk View SE, in theExplorerwindow, double-clickSystem>Policies>System Policies.
- Right-clickSecurity Policy, and then clickProperties.
- In theSecurity Policy Propertiesdialog box, underSingle Sign-On Policy Settings,Use single sign-onshould be set toEnabled.
Remarks
- To check that the user is logged into FactoryTalk Directory, open the Log On to FactoryTalk utility. If a user name is displayed in the Logon Information section of the Log On to FactoryTalk dialog box, the single sign-on user has been set.
- Single sign-on is not supported by the Specify FactoryTalk Directory Location tool. You have to log in every time you use it.
- If the FactoryTalk View SE client is the first product to log into FactoryTalk Directory on a computer, the currently logged-in Windows user will be logged into FactoryTalk Directory and single sign-on will be set if the user is also a FactoryTalk Security Windows-linked user and single sign-on has been turned on in FactoryTalk Security.
- If the user attempting to log on is a FactoryTalk Security user, but not a FactoryTalk Security Windows-linked user, they are logged into FactoryTalk Directory without setting single sign-on.
- For more information about how these features are used in FactoryTalk View, see Chapter 5 in theFactoryTalk View Site Edition User's Guide.
- For more information about single sign-on, seeFactoryTalk Services Platform Help.
Provide Feedback