Advance settings - Other options
The following table shows options in the page.
Option | Description |
---|---|
Maintain client tag connection | Select this check box to allow the client to maintain the tag connections for up to 100 displays. A display loads faster for the operator if its tag connections are maintained. Once 100 displays are reached and new displays are opened, the oldest displays are discarded from the group. This setting will only provide benefit when used in a large system that includes more than 20 View SE clients. This setting can be used to limit the number of tag connections between the client and data server. By limiting the number of tag connections between the client and the data server, memory usage can be regulated on the data server. |
Navigation tracking | Navigation tracking and its settings are only applicable to the navigation button
and its associated navigational commands. Select this if the application uses display navigation functionality. If you do not select this, the navigation buttons configured in the application will not work.
|
Max Number of Displays tracked for Navigation | Input a number between 2 and 50 to set the maximum number of displays tracked for navigation. |
Font Size in History List | Click the down arrow to select an appropriate font size for the items displayed in the History List. |
Always use on-screen keyboard for operator entry | Select this check box to show an on-screen keyboard when the user touches or clicks the user name or password field in the login dialog box, or a string or numeric input field. If this is selected, the on-screen keyboard will be shown for all numeric input objects, string input objects, recipe objects, or Alarm and Event objects on any graphic display the client shows, whether or not the display has been set up to show the keyboard. Note:
The touch keyboard cannot be launched in the RecipePro+ editor if the device has a touchscreen and its operating system is Windows 10 v1511 with tablet mode. |
Hide Update Field button | Select this check box to hide the Update Field button during runtime. |
Allow to get project files from an alternate location | Select this check box to enable the FactoryTalk View SE Client to get HMI project files rom a location other than the HMI server.Select this option if you want to optimize access to HMI project files when HMI servers and clients in an application are connected over a slow-performing network. You can use an alternate location only if the client configuration is for a FactoryTalk View SE network distributed application. The alternate location must be set up manually. |
Provide Feedback