Commands that execute on an HMI server
The following commands can be issued from a
FactoryTalk View SE
Client, FactoryTalk View Studio
, Administration Console, or FactoryTalk View SE
(HMI) Server. They are always run on FactoryTalk View SE
server.- DatalogChangeRate
- DatalogMergeToPrimary
- DatalogNewFile
- DatalogOff
- DatalogOn
- DatalogRenameFile
- DatalogSnapShot
- DatalogSwitchBack
- DerivedOff
- DerivedOn
- EventOff
- EventOn
- RecipeProDownload
- RecipeProUpload
Provide Feedback