Move or resize windows

You can move or resize the main window and any of the editors’ windows.
To move a window:
  1. Position the mouse cursor on the window’s title bar and press the left mouse button.
  2. Holding the mouse button down, drag the window to its new position.
  3. Release the mouse button.
To resize a window:
  1. Move the mouse cursor to a border or corner of the window, then press and hold the left mouse button when the cursor turns to a double arrow.
  2. Drag the window to its new size as you hold down the left mouse button.
  3. Release the mouse button.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal