Add an OPC data server - network station
OPC data servers provide a link between applications and third-party devices so applications can access device tags.
To add an OPC data server:
- InFactoryTalk View Studio, in the Explorer window, right-click the application root, or right-click the area name, selectAdd New Server>OPC DA ServerorOPC UA Server.
- Set up properties as needed. For details, see the product documentation.
- When finished, clickOK.
Remarks
- When adding a data server other than RSLinx Classic orFactoryTalk Linxto a network distributed application, it is best to place the data server in its own area, separate from the area where the HMI server resides. This avoids unnecessary OPC requests and reduces the overall number of OPC transactions between FactoryTalk Directory and the OPC data server.
- When running aFactoryTalk ViewSite Edition application within a Windows workgroup, all Windows users should have Windows Administrative rights assigned to them.
- Direct reference tags can be used to retrieve tag values via aFactoryTalk Linxor OPC data server, from PLC5 controllers and all products in theStudio 5000controller family including ControlLogix, CompactLogix, FlexLogix, DriveLogix, SoftLogix, and GuardLogix controllers.
- Names for the followingFactoryTalk View Studiocomponents do not support extended ASCII characters or Unicode characters: applications, areas, HMI servers, data servers, HMI tags,FactoryTalk Linxshortcuts, andFactoryTalk View Studioapplication files (. SED).
- For information about setting up an OPC server, see the FactoryTalk Help.
Provide Feedback