Add a FactoryTalk Linx data server - network station

To access values in a ControlLogix controller, add a
FactoryTalk Linx
data server that will provide a link, in the form of direct references, between the application and the controller containing the tags that are being referenced.
To add a
FactoryTalk Linx
data server:
  1. In FactoryTalk View SE, in the Explorer window, right-click the application root or an area name, depending upon where you are adding the server, and then click
    Add New Server
    > Rockwell Automation Device Server (
    FactoryTalk Linx
    )
    .
  2. In the
    FactoryTalk Linx
    Server Properties
    tabs, specify the required information for a
    FactoryTalk Linx
    data server.
  3. Click
    OK
    to save the
    FactoryTalk Linx
    data server information.
    For detailed information about the
    FactoryTalk Linx
    Server Properties
    tabs, click
    Help
To modify the properties of a
FactoryTalk Linx
data server:
  1. In the Explorer window, right-click the name of the
    FactoryTalk Linx
    data server, and then click
    Properties
    .
  2. In the
    FactoryTalk Linx
    Server Properties
    tabs, change the information as required, and then click
    OK
    .
Remarks
  • FactoryTalk Linx
    is optimized for use with all products in the
    Studio 5000
    controller family including ControlLogix, CompactLogix, FlexLogix, DriveLogix, SoftLogix, and GuardLogix controllers.
  • When running a FactoryTalk View Site Edition application within a Windows workgroup, all Windows users should have Windows Administrative rights assigned to them.
  • Names for the following FactoryTalk View Studio components do not support extended ASCII characters or Unicode characters: applications, areas, HMI servers, data servers, HMI tags,
    FactoryTalk Linx
    shortcuts, and FactoryTalk View Studio application files (. SED).
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal