Add a copy of an HMI server - network station
You can add a copy of an existing HMI server to a network station application by using the
Copy an HMI server
option, in the Add HMI Server
wizard.
TIP:
The server to be copied cannot be part of the current application. You can either copy a server from another application, or copy one that is not currently part of any application. If you are copying one that is part of another application, make sure that the server is not loaded when you try to copy it.
Names for the following FactoryTalk View Studio components do not support extended ASCII characters or Unicode characters: applications, areas, HMI servers, data servers, HMI tags,
FactoryTalk Linx
shortcuts, and FactoryTalk View Studio application files (. SED).To add a copy of an HMI server:
- InFactoryTalk View Studio, in the Explorer window, right-click the application and selectNew Area.
- In theNew Areadialog box, specify a name and description and clickOK.
- Right-click the area's icon and then clickAdd New Server>HMI Server.
- In theSelect Operationwindow of the HMI Server wizard, clickCopy an HMI server>Next.
- In theSelect Existing HMI Serverwindow, beside theServer namefield, click the down arrow to scroll the list of servers and select one, and then clickNext.
- In theNew HMI Server Propertieswindow, type the name and a description for the new server.
- ClickFinish.
Provide Feedback