RecipeProDownload

Use this command to write the ingredient values of the specified recipe file to the tags in the tag set.
Syntax
RecipeProDownload
<recipe_file
>|<
variable_recipe
> [
/S
status_tag
] [
/R
recipename_tag
]
where
<recipe_file>
is a relative or absolute reference to the recipe file.
<variable_recipe>
is a relative or absolute reference to a tag that represents a recipe file name. You can specify the tag value at runtime.
[
/S
status_tag
] is a relative or absolute reference to a tag that represents the result of the recipe download operation.
[
/R
recipename_tag
] is a relative or absolute reference to a tag that represents the name of the downloaded recipe.
Remarks
If you do not specify the area, the current area is used by default.
This command can be issued from the
FactoryTalk View SE
Client,
FactoryTalk View Studio
, or HMI server, but is always run on the HMI server.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal