Example: RecipeProDownload
RecipeProDownload Chocholate
This command writes the ingredient values of the recipe file
Chocholate
under the current area to the tags in the tag set.RecipeProDownload $Cookie\Recipename$
Cookie\Recipename
is a tag that represents a recipe file name. At runtime, after you specify a value for the tag, for example, Butter
, this command writes the ingredient values of the recipe file Butter
to the tags in the tag set.Provide Feedback