PrevPosition
Moves focus to the object with the previous index number.
This command is run on the currently active display on the
FactoryTalk View SE
Client or FactoryTalk View Studio
that issued the command. It will be ignored when it is issued from an HMI Server or if no display is active.Provide Feedback