Position

Moves focus to the object with the specified index number.
Syntax
Position
<n>
where
<n>
is the object's index number.
Remarks
This command is run on the currently active display on the
FactoryTalk View SE
Client or
FactoryTalk View Studio
that issued the command. It will be ignored when it is issued from an HMI Server or if no display is active.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal