Object Methods dialog box
How do I open the Object Methods dialog box
On a display, right-click an object and select
Methods
.Shows the methods and properties implemented in the selected graphic object. A method is a function that is part of an object.
You can select a method or property and click
?
for more details about the selected item.
TIP:
Use the
Invoke
command to call a method.When you use the
Invoke
command to call a method, you need to specify the name of the object in which the method is implemented.You can copy information from the Methods help and paste it elsewhere such as in the ActiveX Control Events dialog box.
Provide Feedback