Change the appearance of text objects

Use the
Text Properties
dialog box of a text object to change its content, font, colors, style and other properties.
TIP:
A font with two sizes in a display is treated as two separate fonts. Having too many distinct fonts in a display can slow down its general performance.
To change the appearance of a text object:
  1. In
    FactoryTalk View Studio
    , in the Graphics editor, right-click the text object and select
    Properties
    .
  2. In the
    Text Properties
    dialog box, in the
    Genera
    l tab, change the options if required.
    TIP:
    You can also change the size of the text by selecting the text object and then grabbing and dragging its handles until it is the size you want.
    You can also use the
    Ctrl
    key and the
    +
    key to increase font size, or
    Ctrl
    and the
    -
    key to decrease it.
  3. In the
    Common
    tab, change the size, position, name, tooltip text, and visibility if required.
  4. Click
    OK
    .
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal