Paste state properties
After you copy the state properties, you can then paste the copied state properties to one other state or to all states for the object. The selected properties are copied to the new states.
To paste state properties
- InFactoryTalk View Studio, in theGraphicseditor, double-click an object on a display to open its property tabs.
- In theStatestab, in theSelect statelist, click the state you intend to paste the copied properties to. If you are copying the properties to all states, it does not matter which state is selected.
- ClickPaste.
- In thePaste State Settingsdialog box, clickCurrent StateorAll States, and then clickOK.
Provide Feedback