Copy state properties
Use the
Copy State Settings
dialog box to specify the state properties to copy. When you paste, you can paste the copied state properties to one other state or to all states for the object. The selected properties are copied to the new states.To copy state properties:
- InFactoryTalk View Studio, in theGraphicseditor, double-click an object on a display to open its property tabs.
- In theStatestab, in theSelect statelist, click the state whose properties you intend to copy, and then clickCopy.
- In theCopy State Settingsdialog box, select the check boxes beside the properties you intend to copy, and then clickOK.
Provide Feedback