Time and Date Variable dialog box

How do I open the Time and Date Variable dialog box
Below the text field where you want to insert the variable, click
Insert Variable
and select
Time/Date
.
If you are in the
Local Messages
editor:
  1. Right-click anywhere in the
    Message
    column and select
    Edit String
    .
  2. In the
    String Edit
    dialog box, click
    Insert Variable
    and select
    Time/Date
    .
Use this dialog box to insert a time and date variable in a text box. The time and date will change dynamically at runtime.
Embedded variables are case sensitive, and must use the correct format and syntax to work. If you make a mistake, the variable will be treated as text. For this reason, to avoid problems it is better to use the
Insert Variable
button to open a variable dialog box, rather than create or edit embedded variables manually
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal