Insert a string variable
Use the
String Variable
dialog box to create a string variable for a text field.To insert a string variable:
- Below the text field where you want to insert the variable, clickInsert Variable.
- ClickString.
- In theString Variabledialog box, specify the options.TIP:You can include numbers in theLiteral stringoption. However, if the number you want to display requires decimal places or other special formatting, use theLiteral numberoption.
Provide Feedback