Edit a string variable

Use the
String Variable
dialog box to edit a string variable for a text field.
To edit a string variable:
  1. Double-click the string variable syntax in the text box where it has been inserted, or right-click it and then click
    Edit Variable
    .
  2. In the
    String Variable
    dialog box, make the required changes and click
    OK
    .
    TIP:
    You can include numbers in the
    Literal string
    option. However, if the number you want to display requires decimal places or other special formatting, use the
    Literal number
    option.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal