Set up states for an interlocked push button

Use the
States
tab to set up states. After you set up the properties for one state, you can copy and paste the state’s properties to another state or to all states.
To set up states:
  1. In the Graphics editor, in a display, double-click the object to open the
    Properties
    dialog box.
  2. Click the
    States
    tab.
  3. In the
    Select state
    list, click
    State 0
    .
  4. Specify the properties for
    State 0
    as needed.
  5. Repeat steps 3 and 4 for other states.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal