Set up connections for an interlocked push button

Use the
Connections
tab to set up connections.
To set up connections:
  1. In the Graphics editor, in a display, double-click the object to open the
    Properties
    dialog box.
  2. Click the
    Connections
    tab.
  3. Assign a tag or expression to each connection.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal