Interlocked Push Button Properties - Connections tab
The following table shows the options in the
Connections
tab of Interlocked Push Button Properties.
Options | Description |
---|---|
Value | Assign a tag to the Value connection. The Value connection triggers the interlocked push button's action. |
The following table shows other options in the
Connections
tab.Options | Description |
---|---|
Name | This column shows the name of the connection. |
Value update direction | This column shows an arrow to indicate which way data can flow between the connection and the data source. ![]() ![]() ![]() |
Tag/Expression | Type the tag name or expression associated with the connection. If a tag or expression has already been selected, it is displayed here. |
Tag button (...) | Click this button to open the Tag Browser and choose a tag instead of typing the tag name in the Tag/Expression column. |
Exprn button (...) | Click this button to open the Expression editor and create an expression instead of typing the expression in the Tag/Expression column. |
Provide Feedback