Create a string input object
At runtime a string input object allows the operator to type a string that will be written to a tag in an external device or tag database.
To create a string input object:
- InFactoryTalk View Studio, in theGraphicseditor, selectObjects > Numeric and String>String Input.
- Drag the mouse to draw a box the approximate size the string input object is to be.
- In theString Input Propertiesdialog box, specify the tag the string value will be written to.
- In theCommontab, set up how the object will appear at runtime.TIP:Values can also be uploaded from a recipe file or a tag in an external device, to a string input object.If you are using theContinuous updateoption with multiple input objects on a display, for example with a recipe, do not use theDiscardinput option.
Provide Feedback