Create a string display object
Use the string display object to show the current value of a string tag.
To create a string display object:
- InFactoryTalk View Studio, in theGraphicseditor, selectObjects > Numeric and String>String Display.
- Drag the mouse to draw a box the approximate size the string display object is to be.
- In theString Display Propertiesdialog box create an expression or select a tag that will return the string you intend to display.
- If you are using an expression, clickCheck Syntaxto see if the syntax is correct.
- In theCommontab set up how the object will appear at runtime.
Provide Feedback