Set up states for a multistate push button
Use the
States
tab to set up states. After you set up the properties for one state, you can copy and paste the state’s properties to another state or to all states.To set up states:
- In the Graphics editor, in a display, double-click the object to open thePropertiesdialog box.
- Click theStatestab.
- In theSelect statelist, clickState 0.
- Specify the properties forState 0as needed.
- Repeat steps 3 and 4 for other states.
Provide Feedback