Set up connections for a latched push button

Use the
Connections
tab to set up connections.
To set up connections:
  1. In the Graphics editor, in a display, double-click the object to open the
    Properties
    dialog box.
  2. Click the
    Connections
    tab.
  3. Assign a tag or expression to each connection.
TIP:
To provide visual feedback that the
Value
connection has been written to the data source, assign different tags to the
Value
and
Indicator
connections. Configure the data source to pass the
Value
connection’s value to the Indicator connection.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal