DotNetControl Properties - General tab
Use the
General
tab to configure the .NET control. Click <ControlName> Setup
to open the <ControlName> Properties
dialog box where you configure the .NET control's properties, methods, and events and use VBA scripting to interact with them.
TIP:
The DataSource property is not supported in design time or runtime.
Provide Feedback