Create a .NET Control object
Create a .NET Control object to use Windows Forms, WPF, or custom controls of .NET Framework.
To create a .NET Control object
- In the Toolbox, select.NET Control.
- Drag the mouse to create a box approximately the size the control is to be.
- In the.NET Controldialog box, select a control, and then clickOK.
Provide Feedback