ControlName Properties - Events tab

Use the
Events
tab to view event handlers of the .NET control. The list of event handlers varies depending on the type of control. For detailed instructions of each event handler, see the control provider's website or documents.
Unlike FactoryTalk View SE client object model, VBA scripting for .NET Control objects have their own rules and standards. The VBA event sample code shows at the bottom of the dialog box. Click
Copy to VBA
to copy the VBA code and open Microsoft Visual Basic. Select the check box to enable an event, which you can interact with using VBA scripting.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal