ControlName Properties - Properties tab
Use the
Properties
tab to configure properties of the .NET control. The list of properties varies depending on the type of control. For detailed instructions on each property, see the control provider's website or documents.VBA scripting is supported for getting and setting each property. Unlike FactoryTalk View SE client object model, VBA scripting for .NET Control objects have their own rules and standards. The VBA sample code for getting and setting properties shows at the bottom of the dialog box. Click
Copy to VBA
to copy the VBA code and open Microsoft Visual Basic.Provide Feedback