Specify grid settings for a display
You can change the grid settings any time while you are drawing.
To specify grid settings for a display:
- In theGrid Settingsdialog box, specify theAttributesandSpacingoption.
- ClickOK.TIP:Font sizes are not given in pixels. If you want to place text on the grid lines you will have to make the vertical grid slightly larger to accommodate the font. For example, if the font size is 10, and the grid is 10 x 10, the font will not fit correctly. If you make the grid 10 x 14, increasing the vertical grid by 4 pixels, a size 10 font will fit.
Provide Feedback