Grid Settings dialog box options
The following table show options of the
Grid Settings
dialog box.Option | Description |
---|---|
Show Grid | Select this check box to make the grid visible. |
Snap to Grid | Select this check box to make the grid active. |
Grid Color | Click this field and select a color for the grid points. |
Horizontal (x) | Set the horizontal (or x axis) spacing for the grid points in pixels. |
Vertical (y) | Set the vertical (or y axis) spacing for the grid points in pixels. |
Provide Feedback