Save a display

When you save a graphic display, the length of the file name and its complete path can be no more than 256 characters.
The following are reserved names in the object model and should not be used to name a graphic object or display:
Display
,
ThisDisplay
,
Application
,
AlarmSummary
, and
Me
.
To save a graphic display:
  1. In
    FactoryTalk View Studio
    , in the Graphics editor, select
    File
    >
    Save
    or
    Save As
    .
  2. Enter a name for the display and click
    OK
    .
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal