Reduce the display magnification
The
Zoom Out
option on the View
menu reduces the magnification of the display. This gives you an overview of the objects in the display. You can also specify the size with a controlled size.To reduce the magnification of a display:
- InFactoryTalk View Studio, in theGraphicseditor, selectView>Zoom Out.
To reduce the magnification of a display a controlled amount:
- InFactoryTalk View Studio, in theGraphicseditor, right-click anywhere in the display and selectDisplay Settings.
- In theDisplay Settingsdialog box, in thePropertiestab, underSize, selectSpecify Size in Pixels.
- Type the size and clickOK.
- In theGraphicseditor, in the editing window, drag the sides of the display to reduce the size as required.
- Right-click anywhere in the display and selectZoom to Fit. The display is resized maintaining its aspect ratio, or relative sizes and positions of the objects in the display.TIP:Cancel Zoomreturns the display to its original size.If theSizeproperty is set toUse Current Size,Zoom to Fitbehaves the same asCancel Zoom.
Provide Feedback