Edit display runtime properties

The options in the
Properties
tab of the
Display Settings
dialog box define the appearance of a display at runtime. For example, you can specify how the display interacts with other displays at runtime, what buttons and text are shown in the display's title bar, whether the gradient style is used, and so on.
To edit runtime properties settings for a display:
  1. In the
    Display Settings
    dialog box, click the
    Properties
    tab.
  2. Edit the settings presented in this tab.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal