ME EmailSender Control
The ME EmailSender Control provides the system with the ability to send an email via an SMTP server. You can use the control to send a simple email containing a string, an email with an attachment, or an email whose body is contained within an text file. The email is sent via an external SMTP server. The control provides the following features:
- Send an email
- Send an email with an attachment
- Send to separate TO, CC and BCC list
- Customize the sender
- Customize the subject
- Customize the signatureIMPORTANT:Please note you should only use one control per display, and it is suggested to only have one per application.
Provide Feedback