SFC control
The
SFC
control displays the SFC batch structure, which is the same as the FactoryTalk Batch View
Details display page. The SFC
control supports the set of commands an operator can perform on a selected batch or step. The SFC
control generates events when an operator interacts with the running batch. Some property data of the SFC
control is maintained for scripting.Provide Feedback