FullView control

The
FullView
control displays the entire
FactoryTalk Batch View
site, so that an operator can interact with the site using a single HMI control in a
FactoryTalk View SE
display client.
Use the
FullView
control to create, view, and command control recipes, acknowledge prompts and signatures, view equipment phases and diagnostic information, and view profile information. The
FullView
control has some differences from viewing the
BatchesList
control or
PromptsList
control individually. In the
FullView
control:
  • The
    FactoryTalk Batch View
    navigation bar is shown instead of the Diagnostic bar.
  • There is no BaseFilter property.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal