Library of Process Objects

The Library of Process Objects, also referred to as the
PlantPAx
library, contains add-on instructions and associated visualization files that are available to develop applications. The visualization files that are installed with the FactoryTalk View SE installation include HMI faceplates, global objects, images, macros, tags, and local messages.
For more information about the Library of Process Objects, see
Rockwell Automation Library of Process Objects Reference Manual
(PROCES-RM200_-EN-P).
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal