Stop an HMI server and prevent remote clients from starting it
To restore an HMI server, the target HMI server you are overwriting cannot being running.
To stop an HMI server and prevent remote clients from starting it:
- SelectStart > Windows System > Control Panel. In Control Panel, clickSystem and Maintenance> Administrative Tools, and then double-clickServices.
- In the list of services, right-clickRockwell HMI Frameworkand selectProperties.
- In theRockwell HMI Framework Propertiesdialog box, click theGeneraltab, and then set theStartup typetoDisabled.
- Restart the computer.TIP:To restart the computer remotely (for example through Remote Desktop), open Command Prompt, typeshutdown /r, and then pressEnter.
Provide Feedback