WriteOnEnter
Specifies whether to write to the data source when the operator presses an Enter key button object or the Enter key on an external keyboard/keypad, while the Control List Selector is the selected object on the display.
If you select False, the application writes the state value to the data source as soon as a new state is highlighted.
Provide Feedback