Value (ramp button)

A read-write connection. The application keeps a copy of the Value connection on the computer. When the operator presses the ramp button, the application adds or subtracts the RampValue amount from the local Value control value and writes the result to the Value connection tag’s data source.
TIP:
If the RampValue property is a floating point value and the Value control is an integer tag, the application rounds the value before writing it to the control.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal