Value (alphanumeric string)

A write connection. Assign a tag that can support up to 82 characters (bytes). When the operator presses the Enter key, the application writes the alphanumeric string to the tag’s data source.
TIP:
If you do not assign the Value connection, at runtime when the operator presses the button, the string pop-up scratchpad or keyboard does not open.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal