HoldTime
Specifies a minimum hold time for the object. The application will keep the object pressed for this length of time even if the operator releases the object sooner. If you select 0 seconds, the object is reset as soon as the operator releases it.
The hold time should reflect network traffic. Increasing the hold time prevents a very quick object press from being missed by the data source. If the data source is a memory tag, network traffic is not an issue.
Display changes can occur before the hold time has expired. The operator cannot press the object again until the hold time has expired.
Provide Feedback