FactoryTalk Remote Access Manager Authentication

Access FactoryTalk Remote Access Manager as follows:
  1. Once you have created your
    MyRockwellAutomation
    account, sign in to the FactorytalkHub.com webpage and authenticate by entering your MyRockwellAutomation account credentials.
    NOTE: See Create an organization and a domain to learn how to create a MyRockwellAutomation account.
  2. Select the FactoryTalk Remote Access tile, and another authentication is required.
  3. In the authentication window, enter the code sent to the mobile phone that you associated to this 2-factor authentication during the registration of your
    MyRockwellAutomation
    account and access the application.
    NOTE: See Two-Factor authentication for further information on this subject.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal